Part Number: TPA3255
Tool/software:
Hi TI,
Will there be any phase shift from input to output in the class D?
In my project there is a phase shift of 180 degree from input to output.
It is a PBTL configuration
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPA3255
Tool/software:
Hi TI,
Will there be any phase shift from input to output in the class D?
In my project there is a phase shift of 180 degree from input to output.
It is a PBTL configuration
Input - input given to the system from analyzer
Output - Output across the 4 ohm load
Audio_p - Audio input -(INPUT_A)
Audio_N - Audio input-(INPUT_B)
Out_A - Output A from class d
Hi Arjun,
The TPA3255 is an inverting amplifier. Any further phase shift will be dominated by the LC filter.
Regards,
Ramsey
hi Arjun
the phase shift will be there for the analog amplifier.
thanks
jesse