This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5782M: Inquiries about AC Coupling, Dithering, Mute, and the Programmer

Part Number: TAS5782M
Other Parts Discussed in Thread: PUREPATH-CMBEVM

Tool/software:

Hi,

I'm working on a Class-D Amplifier based on the TAS5782M, which I'm going to control its registers using an STM32 MCU over the I2C communication protocol. I've the following questions:

1) The EVM board uses MLCC capacitors for the AC coupling between the DAC_OUT pins and the SPK_IN+ of the amplifier, and the SPK_IN- to the ground. I want to replace the MLCCs with aluminum electrolytic capacitors for higher audio quality, the question is related to the polarity of these caps; as I'm wondering whether there is an internal DC bias at the DAC_OUT or SPK_IN pins that requires careful attention to the polarity. (I'm using BTL Mode).

2) The registers sheets mention the terminology "dithering", which I would like to know more about, and how it affects the audio quality, furthermore, what are AC/DC/DEM dithering, and what should I do with these registers? (a detailed answer would be appreciated).

3) In register 0x08, what does MUTE Control Enable do, what are the PCM to TPA modes?

4) Is there any way to program the TAS series of smart amps directly using a USB to I2C converter? does the PPC3 software generate a hex file or so, which can be used to upload the code to the TAS without using the PUREPATH-CMBEVM board? because I noticed that the PUREPATH-CMBEVM uses the TAS1020BPFB which is an Obsolete part.

Best Regards.