Other Parts Discussed in Thread: TAA5212
Tool/software:
I see the part includes a built-in phase-lock-loop. Specifications are provided at the standard sample rates, for example 96 kHz and 192 kHz.
My question is whether the part can be used in a design which uses a sample rate in that range but is not one of the standard sample rates. For example 100 kHz.
It is not clear from the data sheet whether the part is limited to just the standard sample rates, or may be used at similar sample rates but not a standard rate.
Thank you.
.