This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM6260-Q1: Please recommend the level conversion chip applicable to TDM: 1.2 V → 3.3 V, rate 50 MHz,bidirectional

Part Number: PCM6260-Q1
Other Parts Discussed in Thread: SN74LXC2T45-Q1

Tool/software:

The IO level of the used SOC is 1.2 V.
The IO level of the PCM6260 is 3.3 V.
The maximum bit rate=384(kHz)*32(bit)*4=49.152M

Please help recommend or evaluate:

①Please recommend the level conversion chip applicable to TDM: 1.2 V → 3.3 V, rate 50 MHz,bidirectional.

②We find SN74LXC2T45-Q1,please help us to evaluate whether it can be used in the above scenarios.

Thanks