Part Number: TPA3118D2
Tool/software:
Hello
In our application we planned to use TPA3118D2, but just now noticed that it has a DC protection feature disabling the IC at very low AC frequencies. While such feature is beneficial in audio applications, in our case we have sub-Hz signals that have to be amplified. We also use DC coupled inputs to overcome high pass rejection.
I have a few questions
1. Is there a way to somehow disable this feature or some other workaround to make it work at 0.5Hz or even slightly below it?
2. Are there other ICs with similar spec but without this feature?
3. Does this feature uses output signal voltage or input signal voltage to disable output when the signal is above some threshold for too long ?