Part Number: TAC5242
Tool/software:
Hi Teams,
The customer wants to make a test board to test TI's ADC performance. They don't plan to use SOC, it's too complicated. Can we use the TAC5242 chip to design it in this way, using controller mode, MD3 input a 24.576MHz clock signal or 12.288MHz active clock, and then short-circuit the DOUT-DIN of the CODEC so that the audio signal entering from the ADC can be directly transmitted to the DA channel. This makes it easier for them to test.TAC5242.pdf
Please help to check if the schematic design is reasonable,thanks!