Tool/software:
Hi Ti team,
Could you please help review this schematic ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am seeing AC-coupling capacitors on INxM pins, however I am unable to see any on the INxP pins, can you clarify on the same?
Additionally, the connections on the hardware pins (MD0, FMT0 etc) are not visible on the above screenshot, can you share a screenshot showing the same?
Thanks and Regards,
Lakshmi Narasimhan
Hi,
1) Can you clarify if the device is expected to operate in Master or Slave Mode? There is an MCLK signal connected to MD1 pin, however the MSz seems to be pulled down to GND
2) Can you clarify the "IIS_SCLK" and "IIS_SDA" signals which are connected to the MD0 and MSz pins?
3) Additionally, the MICBIAS doesn't seem to have a decoupling capacitor, please refer to the datasheet for the decap recommendation.
Thanks and Regards,
Lakshmi Narasimhan