This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3255: Value of Input DC block capacitor for low frequency signal(Subwoofer)

Part Number: TPA3255

Tool/software:

Hello Mr or Mrs.

I am designing a subwoofer amplifier using TPA3255.

I have a question about a value of DC block capacitor (DBC).

DBC seems to act as a HPF. It seems that the evaluation board or generally uses 10uF for DC blocking. It seems to be suitable for general mid-range speakers, but I think it is not suitable for a subwoofer that generates relatively low-frequency sounds.

How can I determine the DBC to reproduce an input signal of about 25Hz to 300Hz?