This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS3251: TAS3251 Zobel Network

Part Number: TAS3251

Tool/software:

Hello,

on the TAS3251 outputs we have the following filter network and during our first tests all resistors of the Zobel network burned.

The speaker have an impedance of 6 Ohms.

I told the buying department to buy resistors in the range of 4.7 Ohm to 22 Ohm and capacitors from 1nF to 33nF.

Can you give me any suggestion on which values I should use?

Best regards,

Stephan

  • Hi Stephan,

    If the resistors in the zobel had burnt up, then a likely issue was the power rating of the resistors. Make sure the resistors are rated appropriately for the power expected. Some common zobel circuits for this device are a 1uF and 3.3Ohm or a 220nF and 1Ohm RC circuit.

    Regards,

    Ramsey