Tool/software:
Dear TI experts,
My customer now tests PCM9211 on their own PCB. basic schematic is as below;
1. I2S Input :
RXIN5/ABCKI0 - DSP_HOST_BCK
RXIN6/ALRCKI0 - DSP_HOST_LRCK
RXIN7/ADIN0 - DSP_HOST_SD0
2. SPDIF output :
MPO0
3. Register settings : set 0x33 to address 0x60
TXSSRC[2:0]: DIT System Clock Source Select - 011: AUXIN0
TXPSRC[2:0]: DIT Bit Clock, LR Clock, Data Source Select - 011: AUXIN0
4. I2S Data format :
BCK 2.8225MHz
LRCK 44.1KHz
The problem is, SPDIF output is not detected.
They set 0x03 to address 0x60 then SPDIF output is detected and checked PLL Lock in connected external amplifier, but no sound is detected.
They suspected that SCK is not connected RXIN4/ASCKI0 so they think some settings should be different.
Could you guide me to debug this situation? I attach the schematic review thread 3 months ago for your convenience.
Best regards,
Chase