Tool/software:
Hi TI team & experts,
I’m encountering an issue with the TAS3251 amplifier, and the same behavior occurs on both the TAS3251 EVM and my custom PCB. Here’s the detailed scenario:
-
Initial Setup & Normal Playback:
-
I configured the EQ in PPC3 and successfully initialized the TAS3251 via MCU (using the PPC3-generated script).
-
Audio playback works fine at this stage.
-
-
Problem When Re-initializing During Playback:
-
While audio is playing normally, I try to switch EQ effects by re-running the initialization script (exported from PPC3).
-
After re-initialization, the audio output stops, and no sound is produced.
-
-
Troubleshooting Attempts:
-
The PPC3-generated script includes shutdown & re-enable sequences for the TAS3251, which should theoretically allow seamless re-initialization.
-
I also tried performing an AMP RESET before re-initialization (as suggested in the docs), but it didn’t resolve the issue.
-
Question:
-
Has anyone encountered this issue before?
-
Is there a specific sequence or register setting required to safely re-initialize the TAS3251 during playback?
-
Could this be related to timing, register conflicts, or PPC3 script generation?
Any insights or suggestions would be greatly appreciated!
Best regards,
Roger