Part Number: TLV320AIC3007
Tool/software:
I have observed that when i.e. the LEFT DAC is playing a tone, it is coupling to the path of the RIGHT DAC when the RIGHT path is connected (or any other path than DAC L1) to one of the output with an attenuation of -0.5 dB or more, following the attenuation setting. When at 0 dB the tone is not present at the output.
It is like there is an issue with the supply for the attenuator or internal coupling from the DAC line to any other line?
Is there some way to lower this coupling?