Other Parts Discussed in Thread: TAD5212
Tool/software:
Hi,
I'm evaluating TAD5212 using TAD5212EVM-K.
I'm considering using TAD5212 for 4-channel single-ended output.
On PPC3, when "Stereo Single-Ended" is selected in the Output Config tab for OUT1x in the Playback Config section, the output volume is only 500mVrms with the following settings although it is supposed to be 1Vrms according to the datasheet. With the same settings, when "Mono Single-Ended" is selected, the output volume is 1Vrms as intended.
- Source: DAC Input
- VCOM: 0.6*Vref
- BW: Audio BW
- Drive: Headphone
- Level: 0dB
Also, the waveform of the output of Stereo Single-Ended is less smooth than that of Mono Single-Ended, looks like the resolution is reduced. USB audio is sent with 32bit length, 48kHz fs which are the same values as set in PPC3.
I'd like to know how to get 1Vrms with Stereo Single-Ended.
Regards,
Ayako