Tool/software:
We are currently designing a monitoring speaker in which each speaker has two speakers, a treble and a bass. The impedance of both speakers is 8ohm. We would like to evaluate the use of TAP3225 for design. We would like to consult the following questions:
1. Does TPA3255 and PBTL mode support speakers with an impedance of 8ohm? We want to use two TPA3255, one to drive the treble and one to drive the bass. The former stage uses an op amp to achieve electronic frequency division
2, or we use a TPA3255, using BTL mode, one channel to drive the treble, the other channel to drive the bass, the front stage using electronic frequency division to achieve.
Which solution will have the best performance? Please give your suggestions.
Thank you very much!