Part Number: TPA3255
Tool/software:
Hi Ti experts,
My customer uses TPA3255 to drive linear motor.
Q1. We give the input signal IN_A a high level (6V) DC, IN_B input 1V DC, and the output OUT_A outputs a low level (0V); IN_A inputs a low level (1V), and OUT_A outputs a high level (30V). Is this normal? Or which pin can be used to set the positive and negative outputs?
Q2. When powered on, the OUT pin will have an output voltage, the motor will go down in one direction, and then return to normal. Is there a way to control the amplifier to start slowly when powered on? Or is there an enable pin similar to 3886, which can control the output power by controlling its voltage/current.
Below is our circuit connection, VDD=30V.