This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3131D2: Input range and output range check

Part Number: TPA3131D2

Tool/software:

Hi TIer

We can see the input range is maximum 6.3V in INP INN.

So why we set so low input voltage range under 30V power supply?

My customer have a input signal at max 8V, Do you have more suggest , How to convert this input signal to match our devices?

Thank you very much.

  • Hi Tony,

    This is the input stage to a closed loop amp. The amp has a large gain and the input stage was designed with this in mind. If customer is using a larger signal, then it will need to be stepped down by a resistor divider or a op amp attenuator.

    Regards,

    Ramsey