Other Parts Discussed in Thread: PCM5102A
Tool/software:
Hi Team,
I'm planning on using TPA3221 to drive two 4 ohms 100W speakers in PBTL configuration, so if I connect it in parallel, that would make the effective RL become 2 ohms and the total output power in 10% THD+N is 208W? Would that make sense?
Also, I'm using PCM5102A as the DAC, for a single-ended 2.1Vrms input, what is the best gain setting to maximize the amplifer output power? I'm a bit confused in 9.3.2, the Vrms value of the corresponding gain settings. Does it mean I shall select the matching gain setting for a certain Vrms input?