Part Number: TAS2563
Tool/software:
Hi ti team,
The new project is using TAS2563,Please help check the schematic diagram below. Thanks!

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Customer,
some comments:
1 I2C pull up: please check whether there is pull up at far end.
2 sdout could be used as echo reference signal if needed, of course, you can leave this pin NC if you use other signals as echo reference.
3 as you connect pin 12 to GND, it will work in I2C mode.
4 it's better to add 1k ohm resister on Vsns_N, Vsns_P trace.
5 pin17, it's ok to leave it floating as it is NC pin. but you can also connect it to pin 16 (VBST) to enhance the soldering and the power area.
Br,
Wenbin