Tool/software:
ADC MIC output has attenuation
The values input to ADC MIC through the signal generator are shown in the following figure:

However, after passing through ADC MIC, there is a half attenuation in the output value, as shown in the following figure:

May I ask which configurations can be used to reduce or eliminate attenuation.