Tool/software:
Dear friends,
I would like to interface four electret microphones to a TLV320ADC6140 ADC chip. My question is, what is the best way to go about this for optimal performance?
Should I use a pre-amp circuit, or can I connect directly to the ADC via AC coupling capacitors?
Additional context:
[1] All four microphones will be mounted to the same PCB as the ADC
[2] low noise / high SNR is a key factor... Achieving low phase distortion is even more important.
[3] I would also like to minimise size and cost, so component count is a consideration
[4] Required bandwidth - 50 Hz to circa. 16 kHz.
In summary:-
Do I require a preamp circuit like this:- (?)
Hopefully that is clear - happy to elaborate on any areas if you think I need to.
Thanks!