Part Number: DIT4192
Other Parts Discussed in Thread: DIX4192, PCM9211, DIX9211
Tool/software:
Hello TI Support,
I am developing a device that needs to interrupt AES3 audio broadcasting at a scheduled time to play an analog audio broadcasted in parallel.
Input AES3 stream is 24bit and up to 192 kHz.
I’ve selected the DIT4192 for this purpose, as its features align well with my requirements. Could you please provide guidance on how to use the RXP pin to switch between two audio streams? What is the proper way to convert AES3 differential signal to "encoded" format? My guess is usage of AES3 receiver that produces I2S data. Should i go with DIX4192 or PCM9211 (PCM9211 has ADC which can assist my needs and remove the need of MCU)? Or should i use a relay to keep it simple?
Here is a sketch showing the goal I am trying to achieve:
Thank you in advance for your support.
Best regards,
Genadi Manoilenko