I have a PCM58P Burr Brown DAC that I'm hoping someone might be able to help me out with. My problem involves the DC offset at idle of the single output pin, it's not 0 volts and is causing post dac circuitry to operate lopsided. I'm working on an audio DAC unit and it has 2 chips for 2 channels. One of the units has offset within + - 10mv, which corresponds to the bipolar zero error figure, but I'm not sure if this spec is the one I should be looking at. The other chip has like a .24volt offset, and is thus creating a larger offset at the post dac circuit output. Is this normal operation? I'd think more of a 0 volts dc offset would be normal. Can and do these outputs on these (or other) dac chips breakdown and lose spec? The overall dac unit does work, but only because some DC blocking caps were in place at the final output. Needless to say, the post dac circuit on the .24v offset chip is operating lopsidedly, which is really not a good thing. I wouldn't think I/V converters are meant to operate in this fashion. Think I got everything.