This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS3251: Internal electrical connection of PowerPAD

Part Number: TAS3251


Tool/software:

Hi team,

- What is the internal electrical connection of the powerpad of tas3251?

- is it okay to keep it electrically floated? FYI, The evm has thermal pad between the IC and the heatsink and it is electrically not connected. The datasheet tells user to connect it to ground.

Thanks,

Luke

  • Hi Luke,

    The heat sink should have a good connection to board ground. I don't recommend leaving it electrically floating. Having a good connection to the board ground will have additional help with thermal dissipation. 

    Regards,
    Sydney Northcutt

  • Hi Sydney,

    Thank you for the reply. I understand where your comments come from as it is stated in the datasheet.

    About electrical connection:

    The heat sink should have a good connection to board ground. I don't recommend leaving it electrically floating.

    The thermal pad that was applied to was not conductive and was thick enough that no electrical connection was made.

    Customer was able to confirm fine IC operation without electrical connection on the pad on the EVM. Also, pin test showed there was no electrical connection between the pad and pins. (can you confirm this?)

    They would like to use similar condition as EVM where the heatsink is not electrically connected. (the heatsink will have enough power dissipation.) Will there be any harm in the IC?

    About thermal dissipation:

    Having a good connection to the board ground will have additional help with thermal dissipation. 

    I understand connecting the heatsink to the gnd increases the heat dissipation. Thank you for your comment.

    Thanks,

    Luke

  • Hi Luke,

    The customer can do this if they verify it is okay with their design, but it can introduce large EMI issues. As long as thermals are taken care of the IC will still operate normally but I don't recommend doing this. If there is not any heatsink-PCB ground connection then this heatsink is electrically floating and any noise at device thermal pad will coupled to the heatsink via parasitic capacitance. Then this heatsink becomes a huge antenna and results in EMI problems. 

    I am checking internally on the internal connection of the thermal pad.

    Regards,
    Sydney Northcutt

  • Hi Sydney,

    Thank you for your comments.

    Understood about connecting the heatsink to GND.

    Please let me know if you find anything about the internal connection of the thermal pad.

    Thanks,

    Luke

  • Hi Luke,

    Sure no problem. Yes I will keep you posted when I find out this information. 

    Regards,
    Sydney Northcutt

  • Hi Luke, 

    Internally the power pad has an indirect connection to ground from the lead frame. The heat sink though still needs a good connection to ground externally.

    Regards,
    Sydney Northcutt