This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5827: TAS5827 higher power rating

Part Number: TAS5827
Other Parts Discussed in Thread: TPA3251, , TAS5830

Tool/software:

Hello,

Do you have plans to launch products with a higher power rating compared to the TAS5827? I have seen you recently have launched the TPA3251; it would be great to have such a device with a complete DSP.

It also would be great if you could launch a part which just contains the audio DSP.

Best regards,

Johan

  • Hi Johan,

    Yes we have two digital input devices with a higher power rating than TAS5827 which are TAS5828 and TAS5830 (sampling now). Please see below for a comparison table.  

    Thank you for your feedback! I will pass this information to our Systems team. 

    Regards,
    Sydney Northcutt