This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3255: DC operation in SE mode

Part Number: TPA3255
Other Parts Discussed in Thread: TAS5261,

Tool/software:

Hello,

I have to replace TAS5261 with TPA3255. TAS5261 was used to drive loads like heating or peltier elements. In BTL mode I made a test and connected DC directly to INPUT_A and INPUT_B. I figured out that with an offset of about 3.8V to the inputs and a differential DC signal I get the expected result at the output (with low load). E.g. INPUT_A 3.7V, INPUT_B 3.9V). As the datasheet says I expect a shut down at higher loads. Is it possible to use this chip in SE mode to drive such a load with higher current as 1.5A? Is there any risk to use it in such a way?

Best regards,

Manfred