Part Number: LM4675SDBD
Other Parts Discussed in Thread: LM4675
Tool/software:
Hello TI team,
Please help me with below situation.
I have a LM4675SD based design, which I am using to drive a speaker. please refer to the snap below for schematics

Now, I want to change it to drive speakers of an external monitor [Stereo].
Below are the specs of audio input port of Monitor
Audio Input Range: 2.8V pp
Speakers with 8Ohm, 0.5W (THD+N=10%) x2
3.5mm audio jack
1) How do I make this connection?
2) Should I electrically short "Left" and "Right" signal on the cable?
3) How do I take care of ground connection?
4) Should I use TS cable, as it is mono channel source of audio?
Please suggest.
Regards,
Yashwanth