This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM2912A: PCM2912A operating temperature range

Part Number: PCM2912A


Tool/software:

We are planning to use the PCM2912A in one of our embedded projects for an industrial application and require some clarification to finalize our selection.  

Our application requires a controller chip that supports an operating temperature range of –40°C to +85°C. However, as per the datasheet (Chapter 7.3: Recommended Operating Conditions), the specified operating temperature range for the PCM2912A is –25°C to +70°C.

Could you please advise whether the PCM2912A can reliably operate at –40°C ?

if not, do you have any other USB Audio controller that support –40°C to +85°C operating range