This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320ADC3101: TLV320ADC3101 does not output DOUT

Part Number: TLV320ADC3101


Tool/software:

Hello

I am trying to set up TLV320ADC3101 as a slave to the i2s bus.

I set BCLK = 1.536 MHz, WCLK = 48 kHz without using MCLK.

The MCU can output BCLK and WCLK without any problem.

However, the DOUT signal is not received.

When I checked with an oscilloscope, it is LOW and there is no change.

The reset pin is set to high, and I use two unbalanced (single-ended) microphones.

Below is a reproduction of the register write.

Am I missing something? Is the register write order wrong?

Was it a mistake not to use MCLK?

Any advice would be greatly appreciated.

--------------------------------------------------------------
TLV320_WriteReg(0x18, 0x00, 0x00); // page 0

TLV320_WriteReg(0x18, 0x01, 0x01); // soft reset

HAL_Delay(50);

TLV320_WriteReg(0x18, 0x04, 0x07); // PLL_CLKIN = BCLK
TLV320_WriteReg(0x18, 0x05, 0x91); // Enable PLL, P = 1, R = 1
TLV320_WriteReg(0x18, 0x06, 0x08); // J = 8
TLV320_WriteReg(0x18, 0x07, 0x00); // D (MSB)
TLV320_WriteReg(0x18, 0x08, 0x00); // D (LSB)

TLV320_WriteReg(0x18, 0x19, 0x03); // CLKOUT = PLL_CLK

TLV320_WriteReg(0x18, 0x12, 0x81); // NADC = 1, enable
TLV320_WriteReg(0x18, 0x13, 0x81); // MADC = 1, enable
TLV320_WriteReg(0x18, 0x14, 0x80); // AOSR = 128
TLV320_WriteReg(0x18, 0x15, 0x80); // IADC = 128
TLV320_WriteReg(0x18, 0x16, 0x04); // miniDSP decimation = 16

TLV320_WriteReg(0x18, 0x1B, 0x00); // (slave mode, 16bit, BCLK/WCLK in)
TLV320_WriteReg(0x18, 0x1E, 0x00);

TLV320_WriteReg(0x18, 0x3D, 0x01); // Page 0, Reg 0x3D → PRB_R1
TLV320_WriteReg(0x18, 0x0B, 0x81); // NDAC enabled, NDAC = 1
TLV320_WriteReg(0x18, 0x0C, 0x82); // MDAC enabled, MDAC = 2

TLV320_WriteReg(0x18, 0x00, 0x01); // page 1

TLV320_WriteReg(0x18, 0x33, 0x68); // MICBIAS1/2 = 2.5V

TLV320_WriteReg(0x18, 0x34, 0xCF); // Left = IN2L_P, others off
TLV320_WriteReg(0x18, 0x37, 0xCF); // Right = IN2R_P, others off

TLV320_WriteReg(0x18, 0x3B, 0x5F); // Left PGA
TLV320_WriteReg(0x18, 0x3C, 0x5F); // Right PGA

TLV320_WriteReg(0x18, 0x00, 0x00); // page 0

TLV320_WriteReg(0x18, 0x35, 0x10); // DOUT

// ADC Power up

TLV320_WriteReg(0x18, 0x51, 0xC0)
TLV320_WriteReg(0x18, 0x52, 0x00)
TLV320_WriteReg(0x18, 0x54, 0x00)

TLV320_WriteReg(0x18, 0x53, 0x70)
TLV320_WriteReg(0x18, 0x55, 0x70)

^TLV320ADC3101 circuit

J14 and J17 are connected to each other.

  • Hi,

    Before I take a deeper look at your circuit, I believe this is a PLL issue. Using BCLK as the input to the PLL is fine, but the output clock is too low for the expected output of the PLL. Here is a screenshot from the datasheet:

    K in this second equation is J.D. So, your setting of the input clock=1.536MHz * J.D = 12.288MHz which is much below the expected 80MHz minimum output of the PLL. I would suggest setting R = 8, so then your PLL output = 1.536MHz*8*8.0000=98.304MHz. Then, you can set NADC=4, MADC=4, and AOSR=128. Once you change this, let me know if there are still issues with getting DOUT.

    Best,
    Mir