Part Number: TAS2118EVM
Other Parts Discussed in Thread: TAS2118
Tool/software:
We're currently testing the TAS2118 under the following conditions:
- PPC3 version :TAS2118 PPC3 alpha
- Vbat connected to a power supply set at 5V.
- Load: Actual SPK (4ohm).
- Playback: White noise (output approximately 3V rms).
We've noticed that the EVM shunts down when the power supply reaches 2A.
Even after increasing the Peak current limit setting to 5.1A, it still shunts down. Are there any other settings or protection settings we need to adjust?
Please let me know, if you need more information
Thanks.
Guande
.