This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5822MEVM: TAS5822MEVM

Part Number: TAS5822MEVM


Tool/software:

Hello,

we have the TAS5822MEVM and we are trying to configure and control it with a custom microcontroller.

The two audio amplifier on the boad are configured in "mono" (PBTL mode). The I2C bus from the microcontroller is connected in J19 and J18.

The I2S bus from the microcontroller is connected to the test points: SCLK, LRCLK and SDIN1, while jumpers of the headers J11, J13 and J14 are removed.

We are using the two header J3 and J7 to see which amplifier is being used, but in this situation we found that both header have 2.3 Volt on a pin 2 and 3.3V on pin 1, even if the jumper is not connected.

We would like to know why is the voltage on the header not zero on the pin 2 of J3 and J7. Is it suppose to be grounded when the jumper is disconnected?

Moreover, we would like to know the functions of the following:

S1

J12

and where is testpoint tp2?

  • hi, Michele

    J3, J7 hasn't be connected to GND, they were like below, DVDD also has an cap be connected to GND. if cap be charged, dvdd also has slight voltage.

    you cannot use J3,J7 to judge which amp is working, you can check whether amp's output.

    or you can remove j3 or j7 if you don't want one of them not work.

    S1/J12 is used for select audio source comes from xmos or SPDIF like optical or others.

    thx

    jesse