Tool/software:
Hi all,
I have the following questions about using the PCM1809.
I am currently using the PCM1809 with the following configuration to check the output data.
1) It takes about 185 ms from the input of the BCLK and FSYNC waveform to the value I want to output. Is this normal?
2) Why does this happen? Is there a way to reduce it?
3) Can the CR filter miniature version used in SAR be used to improve it? Or can the decision filter be used?
4) Is there a disadvantage as a side effect of filtering? (Effect on gain, effect on DC offset, etc.)
5) If there is an effect on DC offset, can it be removed by High Pass Filter?
6) The Vref value is set at 2.75v.
When collecting the dump data of PCM1809, it seems that the output is about 10% lower than the sensor output. There is a cable in the middle, so it attenuates slightly (2~3%). What is the cause?
Also, when Vref=2.75v and a sine wave of 3v is input from FG, the dump data shows a sine wave of 3v. What does this Vref mean?
Best Regards,
Ryusuke