Tool/software:
Hi,
We are working on a project where we want to achieve a volume level in the range of -10 dB HL to 120 dB HL with a step size of 5 dB. In the EVM software, there are several negative values in the DAC_L and DAC_R sections of the GUI. I have attached an image which shows these negative values. There is no unit specified for the values in the column, which creates confusion in identifying whether I am working with dB SPL or dB HL.
Another problem I am facing is that I am getting ~ 25 to 30 dB SPL (measured in HIT box) at -78.3 value in the column, which seems to be the last value in the column. Is there any way in which I can program the codec to give an audio profile ranging from -10 dB HL to 120 dB HL?