This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AIC3204: Noise and signal debounce time configuration with AIC3204 CS



Hi,

Hi,

I work on the AIC3204 with AIC3204CS (V2.02)

I think I have found some differences between the configuration given by the software for the noise and signal debounce time and the configuration given by the datasheet.

With a sample ADC of 16Khz  I have calculated the value given by the datasheet and compared with the value given by CS. This is  the comparative table

 

Register 92 Cs signal debounce time Datasheet signal debounce time
0 0 Reserved. Write only default values
1 0,25  = 0
10 0,5 4 ADC Word Clocks=0,25ms
11 1 8 ADC Word Clocks=5ms
100 2
101 4
110 8
111 16
1000 32
1001 64 1024 ADC Word Clocks
1010 128  2048 ADC Word Clocks=128ms
1011 256 2*2048 ADC Word Clocks=256ms
1100 512 3*2048 ADC Word Clocks=384ms
1101 1024 4*2048 ADC Word Clocks=512ms
1110 2048 5*2048 ADC Word Clocks=640ms
1111 4096 6*2048 ADC Word Clocks=768ms

Could you say me which are the good values

Thanks for your help

Best regards

Julien