This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1840: 3.3V is unintentionally input to the shutdown pin.

Part Number: PCM1840

Tool/software:

Hi team,

The shutdown pin is connected to the CPU.
Before the PCM1840 is turned on, the shutdown pin is subjected to a voltage of 3.3V for about 50ms by the CPU's specifications.
Is this problematic for the device?
I checked because the absolute maximum rating was IOVDD+0.3V.

Best Regards,
Ryu.