Tool/software:
Hi all,
The customer is considering this device. So I would like to confirm.
For recording, the ADC Power Control in Page 0/Register 81: ADC Channel Setup Register is set to BIT D7, D6 to 1, 1.
Next, the recording is started to change the Un-muted Register (in Page 0/Register 82: ADC Fine Gain Adjust Register).
The recording is complete,
but after the recording is finished, the ADC Power Control BITD7, D6 is set to 1, 1 and then to 0, 0.
Is it okay that the register changes over time?

Best Regards,
Ryusuke