This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SAYKAL-3P-ALLINONE: Need Help installing the CCS software on the Linux Side. Ignore the Part Number.

Part Number: SAYKAL-3P-ALLINONE

Tool/software:

Hello, 

   I am trying to install CCS on Redhat Linux 8. It looks like there is a gcc dependency and it needs to be 3.3 which RHEL 8 does not. 

   Is there a version you can send me that is supported on Redhat Linux 8.7 and 8.10? 

   With that being said the version I installed also is not supported on Redhat 9 as I tried that as well. glibc is OK but libtinfo.so.5 is not Redhat Linux 9. So it did not work either. 

   I would rather have a version that is supported on RHEL 8. I got an error when trying anyway and it for some reason tried to access udev.service which is not running on our OS. Just curious as to why it needs to restart this service specifically. 

Thank you,
Steven Amalfitano

Lockheed Martin Corporation

Software Engineering Staff