Other Parts Discussed in Thread: TAS5827,
Tool/software:
Hello,
I have a portable speaker product that uses 2 TAS5827 amps (one for mono woofer, one for stereo tweeters). During the earlier stages of the project, we were tuning using 2 TAS5827 EVMs that were connected using the IO-EXT pins. However, we have been having a lot of trouble using the EVM to successfully tune the DUT.
Amp A on the DUT has been configured to use I2C address 0xC2 and amp B uses address 0xC6. When we connect the DUT to board A using the I2C pins and initiate the connection in PPC3, we typically get an error saying that "device B could not be reached". If we go into in-system tuning mode using the above addresses, PPC3 will get stuck trying to load the amp settings onto the DUT.
Are you able to tell what is going wrong? Is there a particular jumper configuration that would allow what we are trying to do?
Thank you,
Elliott R