This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM6240-Q1: Total Signal Chain latency

Part Number: PCM6240-Q1


Tool/software:

Hi Team,

I'm trying to calculate the signal chain latency of the PCM6240 and I want to make sure my reasoning is correct. 

The Fsync is at 48kHz, and all the modified register settings are shown below. 

Adc_RegCfg gPcm6240RegInst0[] =
{
    /* Page select 0 */
    {0x00, 0x00},
    /* Reset */
    {0x01, 0x01},
    /* Page select 0 */
    {0x00, 0x00},
    /* Disable sleep */
    {0x02, 0x09},
    /* High impedance for unused cycles */      //word length 32 bits
    {0x07, 0x31},
    /* 1 BCLK delay between FSYNC and data */
    {0x08, 0x01},
    /* CH1 at slot 0 */
    {0x0B, 0x00},
    /* CH2 at slot 4 */
    {0x0C, 0x04},
    /* CH3 at slot 1 */
    {0x0D, 0x01},
    /* CH4 at slot 5 */
    {0x0E, 0x05},
    /* Set micbias to 5v */
    {0x3b, 0x70},
    /* CH1_CFG0: AC-Coupled , single-ended, LINE input */
    {0x3c, 0xA0},
    /* CH2_CFG0: AC-Coupled , single-ended, LINE input */
    {0x41, 0xA0},
    /* CH3_CFG0: AC-Coupled , single-ended, LINE input */
    {0x46, 0xA0},
    /* CH4_CFG0: AC-Coupled , single-ended, LINE input */
    {0x4b, 0xA0},
    /* Input channel enable */
    {0x74, 0xF0},
    /* Power up micbias and power up all ADC channels */
    {0x75, 0x60},
};

Based on the datasheet, my understanding is the latency from the input signal to when it is seen on the TDM line is given by the below diagram:

By default,

  • PGA set to 0 DB
  • Phase Calibration set no delay
  • Decimation filter: Linear phase Decimation
  • HPF: cutoff of 0.000025 * fs
  • Gain Calibration set to 0 DB
  • Channel summing mode disabled
  • Biquad Filters:
    • Unsure on this
  • Digital Volume Control set to 0DB

My understanding based on the datasheet and the above parameters, is that the only thing that introduces delay in the system is the Decimation filter.

Table 24 states that the group delay would be 17.1 x (1/fs) = 365.25 us?

Is the above assessment accurate or are there additional delays caused by the other stages of the signal chain that need to be accounted for?

Additionally, because there is a 1 BCLK delay configured, is there an additional latency in result of the TDM output that needs to be accounted for?