Part Number: TLV320ADC3140
Tool/software:
Hi,
1. The signal from the microphone is input to INxP in a single end. I would like to know the circuit design of INxM in this case. A capacitor is installed in INxM as shown in Figure 31 in the datasheet. Is there a recommended constant value for this capacitor?
Currently, a capacitor with the same value as the capacitor connected to INxP is installed.
2. For single-end input, is it appropriate to set GPO_CFG0 [3:0] to 0d (disabled)?
3. Other than CH1_IMP [1:0], are there any other registers related to the frequency characteristics and signal-to-noise ratio of the input signal?
Best Regards,
Nishie