Tool/software:
As you mentioned earlier, the open-loop output impedance change might affect stability but both datasheet (SBOS058A and SBOS058B) show 10Ω at 10kHz, also their capacitive load graphs (Rev A Fig. 26 vs. Rev B Figs. 5.23, 5.24) look consistent.
However, Rev B includes results with 0Ω, 24Ω, and 51Ω output resistors. In our circuit with Rev A, we didn’t use any output resistor to control overshoot. We want to confirm: for Rout = 0Ω, can we expect the same output with both revisions, or is it now must to add a 24Ω or 51Ω resistor when using Rev B?