This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1841-Q1: Question about electrode tip height

Part Number: PCM1841-Q1


Tool/software:

Dear TI package engineers,

PCM1841QRGERQ1 is VQFN (RGE) | 24.
However, the package dimension drawing on the datasheet does not include the dimensions of the side electrodes.
What are the electrode heights and tolerance dimensions for the external side leads?
e.g. : 1mm±0.2mm

Please refer to the attached explanatory drawing.
Regarding the height of the electrode tip of PCM1841QRGERQ1.pdf

Thank you.
Junji,Regarding the height of the electrode tip of PCM1841QRGERQ1.pdf