Has any one found out what the AVCC pin draws for max current? Also does anyone know what output current is available from VREG? I couldn't find these specs in the data sheet.
Mark Allie
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Has any one found out what the AVCC pin draws for max current? Also does anyone know what output current is available from VREG? I couldn't find these specs in the data sheet.
Mark Allie
Mark,
This pin is very low current draw, on the order of a few mA.
VREG is not to be used to drive external circuitry...
-d2
Thanks for the quick response. A few mA of current draw on pin AVCC is great. About VREG: I did read the data sheet espectially about not driving external circuitry with VREG. I want to use VREG for activating the MUTE and SHDN# pins on the 3106. They are not listed in the suggested pins that can be driven by VREG. I also noticed that the current draw on MUTE and SHDN# are on the order of 100uA where as the other pins (gain0, gain1 and SYNC are on the order of 1uA. To me the MUTE and SHDN# pins are not external circuitry but they are also not listed in the data sheet as pins that can be driven by VREG. So I want to know can VREG drive the 100uA or so per pin for these 2 pins? This is why I asked the question about the output current available from the VREG pin.
Mark Allie