This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5815: About Audio Formats

Part Number: TAS5815
Other Parts Discussed in Thread: TAS2574,

Tool/software:

Hi team,

Audio data format: I2S, Left Justified, 32bit length, 64Fs

The following is a description of each channel in the attached image.
CH1: SCLK
CH2: DATA
CH3: LRCK

  1. From the Timing Requirements, it is assumed that the tLS item specifies the rise time of SCLK from the rise/fall of LRCK.
    In the following image, this would be approximately 354.396ns?



  2. In that case, would SCLK, which is rising at the same timing as LRCK, ever be recognized as the first bit clock depending on the variation in the value of tLS?
  3. In such a case, should we invert the clock to accommodate this?
    In that case, I am concerned that we will not be able to comply with the tSU regulation.
    Although the waveform below is a pseudo-inverted SCLK waveform using the oscilloscope function, the measured value is approximately 6.3838 ns compared to the specified value of 8 ns, which does not comply with the regulations.
    Is the manufacturer's recommendation to invert the clock and adjust the DATA timing so that tSU can be observed?

Best Regards,
Ryu.