Tool/software:
Hi,

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi,

Hi Alan,
Can you share the schematic of the ADC section, to have a look at the inputs being provided to the ADC?
Also, to confirm the configuration, can you provide a readback dump of all the registers configured?
Thanks and Regards,
Lakshmi Narasimhan
The ADC is on the EVM board, so the schematic is on page 21 of this: www.ti.com/.../sbau335.pdf
I connected an AWG to IN1 differentially and generated 1 kHz, 1.4 Vpp on each channel (with some 0.7 Vdc offset, but it's AC coupled), 180deg offset between channels.



This is the recording waveform of me enabling the first channel of the AWG and then the other one. (I also verified the raw samples reach those close to +- 2^31 values). In the second half of the recording we are almost reaching fullscale, but each input is only receiving 1.4 Vpp, so 1 Vrms differential amplitude.

Here's the register dump after init.
I (4728) ADC_ASI_OUT_CH_EN: 10000000
I (4768) ADC_ASI_CFG0: 00110000
I (4808) ADC_ASI_CFG1: 00000000
I (4848) ADC_ASI_CFG2: 00000000
I (4888) ADC_DSP_CFG0: 00000000
I (4928) ADC_DSP_CFG1: 00000000
I (4968) ADC_IN_CH_EN: 10000000
I (5008) ADC_ASI_CH1: 00000000
I (5048) ADC_ASI_CH2: 00000001
I (5088) ADC_CH1_CFG0: 00000100
I (5128) ADC_CH2_CFG0: 00000000
I (5167) ADC_CH1_CFG1: 00000000
I (5207) ADC_CH2_CFG1: 00000000
I (5247) ADC_SHDN_CFG: 00110101
I (5287) ADC_BIAS_CFG: 00000000
I (5327) ADC_PWR_CFG: 11100000
Thank you,
Alan
Hi Alan,
One possible reason for the code wrap at half the rated full-scale could be a mismatch in the ASI output configuration. I see that you have wired out the ASI lines from an external controller to the EVM. The ASI_CFGx values indicate that device is programmed for TDM protocol with TX_OFFSET = 0. If, say, the external controller is sourcing I2S signals, or is expecting a 1 clock of TX_OFFSET, that can result in a bit shift, eventually causing code wrap.
If you are using EVM, you would be having the ACMB as well. Considering that the ACMB provides TDM signals, you should not see the code wrap if this indeed is the root cause. You can:
1) Verify the recording with ACMB + EVM, using the above configuration
2) Verify that the protocol programmed to the device in ASI_CFG0 (TDM, I2S, LJ) matches the signals provided to the BCLK/FSYNC pins from the external controller.
Thanks and Regards,
Lakshmi Narasimhan
Hi Lakshmi,
This was it. I changed ASI_CFG1 to add that 1 BLCK TX_OFFSET and it works perfectly. The TDM driver lib I was using defaulted to the offset protocol and I hadn't realized that. Thank you so much for your help!