Hi All
Designing AGC functionality for the PCM3070 In the PPS (Home Audio), give me two different AGC solutions.
I can use the AGC part of the Decimator, by editing the runtime properties of the decimator, and use a separate AGC block found under "dynamic processing".
Could i ask you to elaborate on the differences btw the two blocks ?
I see in the datasheet that the AGC will operate the analog gain stage prior to the decimator.
I assume that the "Decimator AGC" will operate on the analog PGA, and that the separate AGC block is purely digital. Is this correct ?
Finally PPS seems only to support "Decimator AGC" on both channels simultaniousley. I would like to use it only on one channel. Can i simply enable the "Decimator AGC" and then disable it for one channel simply by overwriting the I2C register for the channel manually (Page 0 bit 7 of either Reg 86 or 94) ?
Thanks in advance
BR
Jesper