Part Number: TAS2563
Tool/software:
Hello,
I am working with TAS2563 and currently trying to design the production test sequence. After reading the end system integration guide (slaa954), our thought was to use ROM mode for running calibration (factorytest program). This results in getting failures due to the measured parameters showing wrong values:
TAS2563 calibration values:
DevA Re = -0.00 Ohm
DevA F0 = 1893.05
DevA Q = -0.00
DevA rms_pow = 0x00000000
DevA t_limit = 0x2EE00000
SPK A Calibration fail : Re is too low (limit: 2.00).
SPK A Calibration fail : F0 is too high (limit: 450.00).
Factorytest however, works fine with tuning mode. So my question is:
1. Is it expected that factorytest doesn't work when the smartamp runs on ROM mode?
2. Which mode is recommended to use when running factorytest? Is it tuning mode? Do we need to create a special snapshot where all the tunings (EQ, DRC, etc.) are turned off except the characterization?
3. When is it beneficial to use ROM mode?