Part Number: TAS5828M
Tool/software:
Hello. We need as many static equalization bands as possible for our use case, so no DRC, AGL, etc is needed.
What is the maximum count of BQs that can be used in TAS5828M DSP at 48/96k 2.0?
Going by the block diagram in PPC3 in base/pro 2.0 48k there is:
12 BQs in main EQ,
1 BQ in low level EQ in DPEQ, with sense EQ set to 0 so only the low level path is always active,
4 BQs in DRC mid band, with high band and low band muted, so only the mid band is always active.
2 BQs in Post EQ1
2 BQs in Post EQ2
So 21 static BQs, is that correct?
At 96k a lot of these are not available in PPC3, but the registers are still there as per https://www.ti.com/lit/pdf/SLUUDB4 pages 29 - 31. Is that true or is the table name a typo?
What is the behavior of the DSP if the internal processing rate is set to 96k and BQs in book 0xAA page 5 0x30 - 0x7C, page 6 0x08 - 0x54, etc (DPEQ, DRC) get written?
What is the maximum count of BQs that can be used at 96k?
Is there a processflow / hybridflow with pure EQ or FIR?