Other Parts Discussed in Thread: TPA4861, PCM1772
I'm working on a design using the PCM1772 DAC and TPA4861 amplifier. My question is how to interface between them. Do I need an LPF as shown in the PCM1772 datasheet? Or can I connect directly between them?
If I need an LPF, how do I design one? I found the filters in the DEM-DAI1772 User's Guide -- would these be appropriate?
My first shot at this design did not have an LPF. For the gain components, I used Ci = 1uF, Ri = 15K, Rf = 11.8K (gain of 1.57 V/V). It is at least mostly working -- can't tell at the moment if the distortion on it is a hardware or software problem.
Other comments? Thanks...