This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F169 v.s. AIC3254-EVMK via I2C



Hello,

I try to use I2C to download code into AIC3254 from MSP430F169.

Is the 7-bit Device Address of AIC3254 is 0011000 , the 8-bit register address means the reg_off,

and the 8-bit register data mean the reg_val?

If so , how can I determine I would like to write or read via SDA?

Do I need to shift the reg_off before put in the 8-bit Register Address?

Hope for your reply.

Best Regards,

Steve.