PCM1808-Q1:intermittent noise every 4 seconds

Other Parts Discussed in Thread: PCM1808-Q1, TAS5548, PCM1808

Número de pieza: PCM1808-Q1

Herramienta/software:

Greetings.

I'm working on a degree project involving the TAS5548 and the PCM1808. After various configurations due to noise, I realized the problem is with the PCM1808-Q1. I used to use the PCM1808, but it generated more noise. Then I switched to the PCM1808-Q1. The difference was noticeable, but every 4 seconds it generated a small pulse and a beep simultaneously on the DOUT output. Why does this happen, and how can I avoid the noise so the TAS5548's PWM signal doesn't oscillate?